The firmware update file below, DSO3000_Series_USB_Host_Module_Update, can be installed to fix a color printing problem. This firmware update was tested only for the HP Deskjet 6490 printer.

Requirements:

  • USB flash drive, 128 MB or less.
  • N2865A USB host module attached to the 3000 Series oscilloscope.

To update the USB host module firmware:

  1. Download the file below to the USB flash drive.
  2. Attach the flash drive to the USB host module (which must be attached to the 3000 Series oscilloscope). The 3000 Series oscilloscope may be powered up or down.
  3. When powered up, the 3000 Series oscilloscope should recognize the flash drive and display a dialog showing the update progress. There is no message that indicates the update was successful.
  4. Once the progress dialog disappears, power down the oscilloscope, remove the flash drive, plug in the printer, wait a few seconds, then power up the oscilloscope.
  5. Print.
Keysight는 가능한 최신 버전을 사용하는 것을 권장하며, 최신 버전에는 현재 사용 가능한 가장 최신 버그 수정 및 보안 패치가 포함되어 있습니다.
릴리스 날짜 버젼 버전 설명
2008-11-21 n/a Firmware update for the N2865A USB host module (for Keysight 3000 Series oscilloscopes).
릴리스 날짜 버젼
2008-11-21 n/a
Version Description
Firmware update for the N2865A USB host module (for Keysight 3000 Series oscilloscopes).

다운로드 방법

  • See Above

설치 방법

  • See Above

라이센스

  • Does Not Require a License

Installs on: Instrument

선결 조건

  • See Above

지원되는 계측기

  • N2865A
사용 가능한 소프트웨어 버전이 없습니다.
SHOW MORE