Installable Instrument:
This firmware is installable into the following instrument.

  • E5270A
  • E5272A
  • E5273A

Firmware Revision:
A.01.07

Resolved Defects:
The following feature is available.

  • I measurement calibration limit was changed to relax restriction according with hardware specification

Update Instruction:
See the update appl.txt file included in the zipped file.

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2004-11-15 A.01.07 E5270A Series Firmware Rev.A.01.07
Veröffentlichungsdatum Version
2004-11-15 A.01.07
Version Description
E5270A Series Firmware Rev.A.01.07

How to Download

  • See the update appl.txt file included in the zipped file.

How to Install

  • See the update appl.txt file included in the zipped file.

Lizenzierung

  • Does Not Require a License

Installs on: Instrument

Voraussetzungen

  • See the update appl.txt file included in the zipped file.

Supported Instruments

  • E5270A, E5272A, E5273A
Keine Softwareversion verfügbar
SHOW MORE