Library Installation:

Install this software update in the following instrument.

  • B1500A with EasyEXPERT

Import this application test definition into the EasyEXPERT Library.

The initial release of "NBTI(Id)" application test definition is imported in the new "NBTI" library category.

The second release of "NBTI(Id)_2" application test definition is imported in the new "NBTI" library category.

Revision:

This application test definition runs on EasyEXPERT A.02.10 or later.

Documentation:

Refer to the application note in Documents and Downloads below.

Timing on-the-fly NBTI(Id) 2.zip file includes a readme for the second release features.