What is the resolution of the VGA monitor output from the 8560EC Series spectrum analyzer?
The resolution is 640 x 480 pixels on a standard 15-pin VGA connector. This connector is located in the upper left corner of the rear panel (J1) and is always active.