Is VEE able to interpret "," as decimal point in Formula box running under German Windows?
German version of Vista and Windows XP interprets "," as decimal point.
However usage of "," inside the formula box results in wrong calculation. Such as: "0,5+0,5" in the formula box with the intention for comma as decimal point. The result is 5 (which is invalid with the anticipated result as 1).
This is caused by VEE's usage of "," as a parser, resulting in another statement .
VEE's formula box will continue to adhere to internation standard notation using "." as the decimal point, while using "," as a separator. As a workaround, we advice German customers to use "." as the decimal point.