What is the Difference Between the 8164A and the 8164B?
Frequently Asked Questions (FAQs)
Summary
What is the difference between the 8164A and the 8164BQuestion
What is the difference between the 8164A and the 8164B?
Answer
There are two main differences in the 8164B unit:
- Faster processor
- Faster IEEE 488 chipset which enables a faster throughput that is 30 % faster for large block transfers