Starting Download..
save Save

What is the Difference Between the 8164A and the 8164B?

Frequently Asked Questions (FAQs)

Summary

What is the difference between the 8164A and the 8164B

Question

What is the difference between the 8164A and the 8164B?

Answer

There are two main differences in the 8164B unit:

  1. Faster processor
  2. Faster IEEE 488 chipset which enables a faster throughput that is 30 % faster for large block transfers
Was this helpful?


Didn't find what you're looking for?