How do I install the X8711A software?
It is recommended to use the installation wizard to install the software components. The installation wizard can be found at keysight.com/find/X8711A under Technical Support then the Drivers, Firmware & Software tab. There is both an on-line and off-line installation download available.
If there is a need to manually install the software components, refer to the instructions.