How to measure temperature with the AUXILIARY METER function of the U1602A/U1604A handheld Oscilloscope?
Temperature can be measured using the temperature meter mode under the AUXILIARY METER function of the U1602A/U1604A handheld Oscilloscope. Temperature measurement requires a temperature adapter to work with the instrument.
The U1586A Temperature adaptor is offered as option accessories. More information on the accessories can be found at the "Options and Accessories" tab of this website.
Please ensure the DUT test range is within the measurement operating range of both main instrument and the accessories, when performing the measurement.