Starting Download..
save Save

What is the difference between E2731A & E2731B or E2730A & E2730B tuners for 89600S vector signal analyzer?

Operational "How to" Guides

Summary

What is the difference between E2731A & E2731B or E2730A & E2730B tuners for 89600S vector signal analyzer?

Description

There are no visible differences, but there is a performance difference relating to the local oscillators. In order to phase-lock two RF channels, the LO's must be connected between two tuners and, in order to obtain the performance necessary to accomplish this, the tuner performance had to be adjusted. Therefore, the revision rolled from A to B. Phase-coherency can only be obtained with two E2730B or two E2731B tuners in a two RF-channel system (89640A or 89641A).

Both A the B tuners are compatible with all 89605 input modules and E1439 ADC modules.

See Also

Hardware Upgrades for 89600S VXI Systems
Was this helpful?


Didn't find what you're looking for?