Can I export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to my PC?
No, you cannot export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to your PC. There is no direct transfer of the waveform saved. The waveform saved in the internal memory can only be viewed on the oscilloscope's onscreen LCD display.
If you wish to save the data in .svw, you should purchase the handheld oscilloscope with the option-001. This will enable you to save the waveform in the external USB flash memory when performing the measurement.
IMPORTANT NOTE: Option-001 has to be specified when placing an order as it cannot be retrofitted on completed or shipped units.