Can I use the 16092A with the 4395A/4396B/4287A/E4991A?
Operational "How to" Guides
Summary
Can I use the 16092A with the 4395A/4396B/4287A/E4991A?Description
Yes, you can use the 16092A with the 4395A/4396B/4287A/E4991A.
In order to use the 16092A with these instruments, it is necessary to set the Electrical Length to 3.4 mm by using the "user fixture" menu of the respective instrument.
For the details about how to define "user fixture", please refer to the following instrument manuals.
4395A Operation Manual (Page 7-17)