Can I use the Quick Print button to quickly save my waveforms into the USB thumbdrive?
Yes, but with Keysight InfiniiVision 5000/6000/7000 Series oscilloscope software version 5.10 and above you have to enable the feature:
- Make sure you have the latest firmware for the oscilloscope (version 5.10 and above). See: InfiniiVision 5000/6000/7000 Series Oscilloscope Software
- Press the Save/Recall key on your oscilloscope. Then, press the Quick Print softkey to enable the feature.
- Press the Save softkey, then the Format softkey, to select the format.
- Plug in your USB thumbdrive.
- Acquire a waveform; then, press the Quick Print key (or Print key on the 7000 Series oscilloscope) to quickly save your waveform.