What is the Difference Between the 8920B's EVM1, EVM10 and Peak EVM?
There are three different EVM measurements available with the Keysight 8920B Option 80X:
- EVM1 - rms average EVM of one entire burst (standards specify rms).
- Peak EVM - peak EVM of one entire burst.
- EVM10 - rms average EVM of first 10 symbols of 10 bursts.
(c) Copyright Keysight Technologies 1999, 2000.
This information is subject to change without notice and is provided "as is" with no warranty. Keysight Technologies shall not be liable for any direct, indirect, special, incidental or consequential damages in connection with the use of this material.