Fixing Error 772 on the E1441A Arbitrary Waveform Generator
There was a production problem with the E1441A cards in 1998 where no valid setup was stored in non-volatile memory location 0. This caused the error 772 (non-volatile memory error) to occur. The easy fix for this problem is to send the following three commands to the instrument:
*RST
MEM:STAT:REC:AUTO OFF
*SAV 0
These commands will cause a valid entry to be stored in memory location 0, and the problem will be permanently fixed.
This problem was corrected in production in June, 1998.