Is there any effective way to measure the impedance of a pressure sensitive SMD component (ex. a ferrite bead) with the 16196 series or 16197A test...
In order to measure a pressure sensitive device, the pressure applied to the DUT by the test fixture needs to be carefully controlled. When using the Keysight 16196 series or 16197A test fixture, the pressure applied to the DUT can be adjusted by modifying the fixture. For the details of the pressure adjustment method, please refer to the following document.
Study about the measurement for small SMD which the impedance are pressure sensitive