8903A, 8903B, 8903E Comparison
The Keysight 8903B is the replacement for the Keysight 8903A. Here are the differences in the Keysight 8903B:
1. True Balanced Input to the Analyzer
2. Front Panel Switchable Detector, rms-to-Average
3. Quasi-Peak Detector, Accessible by Special Function
4. Lower Noise in the Analyzer Portion
5. Switchable Impedance, 50-600 Ohms, by Special Function
6. Voltage Measurements in dBm into 600 Ohms
7. Choice of Two Bandpass Filters from a Menu of 6 (8903A had Options 010 and 051)
The 8903E is simply the analyzer portion of the instrument; no source included. It has the same specifications as the analyzer portion of the 8903B. Not having a source, it cannot do signal to noise ratio; it has a special "notch-lock" function to enable measurement of SINAD and distortion.
Refer to Filer Options for additional information. Filter options are the same for the 8903B and 8903E:
(c) Copyright Keysight Technologies 1997, 2000 All Rights Reserved.
This information is subject to change without notice and is provided "as is" with no warranty. Keysight Technologies shall not be liable for any direct, indirect, special, incidental or consequential damages in connection with the use of this material.
Learn more about Keysight Audio Analyzers