Why am I getting a reading instead of zero when using U1252A/U1253A frequency counter measurement function although no measurement was done…
After the probes are connected to the U1252A/U1253A, the measured value will be automatically zeroed. Please take note that this behavior does not affect the measurement accuracy or performance of the unit as the probes must be connected to make measurements.