Do I need an extra driver besides the Keysight IO Libraries Suite to make my 82357B USB/GPIB Interface work?
Yes, the 82357B requires an external driver to be installed even though it is compatible with the Keysight IO Libraries Suite 14.2. Users can install the driver from the CD shipped with the 82357B, or download the driver from the Keysight website at https://www.keysight.com/us/en/support/82357B/usb-gpib-interface-high-speed-usb-2-0.html
However, if you are using the Keysight IO Libraries Suite 15.0, it will automatically detect the 82357B without requiring a separate driver installation.
Last Updated: 01October, 2007