Why won't my FieldFox Turn On?
Most often occurs when battery completely discharged. Complete the following steps:
- Remove the battery and external power from the unit.
- Connect external power from the unit.
- Turn unit on.
- Insert the battery after the unit has successfully powered on.
Recommendation: Upgrade to the latest firmware, this will update the power on/off firmware in the microcontroller.
If this work around does not correct the problem for older units, see Keysight Service Note N9912A-03 for required hardware modification.
For more information about Fieldfox handheld RF and microwave analyzer, please visit FieldFox Handheld RF and Microwave Analyzers.