How long does the system user alignment of my PSA EMI Measurement Receiver take to run?
There are three different softkeys on the internal user alignment menu that will execute the internal alignments. These three softkeys give the user the option of doing either of the two signal path alignments individually or both at the same time. So, the time that the user alignments will take will depend on what is selected. Below is a table with the approximate times for each of these three selections.
User Alignment Times | ||
---|---|---|
Softkey | Signal Path Aligned | Approximate Time To Complete |
Align 9 kHz to 30 MHz | Conducted | 1 Minute |
Align 30 MHz to 1 GHz | Radiated | 31 Minutes |
Align 9 kHz to 1 GHz | Conducted & Radiated | 32 Minutes |