How can I configure to output continuous arbitrary waveform?
An arbitrary waveform can be created with the B2901/02/11/12A by making use of its List Sweep Mode.
The waveforme which is created with its List Sweep Mode can be outputted multiple times by specifying ARM Count.
In order to source continuous arbitrary waveform it is required to set the ARM count to INFINITY.
Please refer to the following material in detail.