N1915A Peak Power Meter Test Adaptor

Technical Overviews

Product Description

The Peak Power Meter Test Adaptor (PPMTA) is an instrument specifically designed to test peak power meters. It is capable of applying voltages, presented at its input, to the power meter with the same signal conditioning as the meter would expect from a peak power sensor. The use of the PPMTA is a convenience as it allows rudimentary checks of the signal path to be carried out as if the input signal was RF power because the meter treats it as if it were a sensor and scales any input voltage to Watts or dBm. The role of the PPMTA in the measurement is to simply apply the appropriate signal conditioning to the voltage supplied by the voltage source. A peak power sensor has a pair of detector diodes that present a differential voltage, related to the applied RF power, to a differential amplifier, which in turn drives a differential voltage to the meter input. The PPMTA has an XLR connector in place of the diode pair and thus allows a differential voltage from an external source to be applied to the power meter.

Environmental Specs

Keysight N1915A is designed to fully comply with Keysight Technologies’ product operating environment specifications. The following are the summarized environmental specifications for this product.

Evolving

Our unique combination of hardware, software, support, and people can help you reach your next breakthrough. We are unlocking the future of technology.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.