Case Studies
Car Manufacturer Speeds Ahead with Automotive Ethernet Compliance Solution
A fast, reliable, and lightweight physical network is essential for data-heavy applications in advanced driver-assistance systems (ADAS) and vehicle-to-everything (V2X) capabilities. A top global car manufacturer needed to find ways to innovate its designs while reducing cost and weight. It selected the well-established Automotive Ethernet standard to achieve its goals, and turned to Keysight for test and measurement solutions to meet its design goals.
This car manufacturer is racing to bring the super-connected car to the broader medium-priced market. It envisions its new model equipped with artificial intelligence and state-of-the-art over-theair (OTA) connectivity.
These applications range from automatically turning on smooth jazz for the ride home to warming the oven for dinner while concurrently downloading the latest firmware upgrades.
The car maker’s design team developed a 100BASE-T1 Ethernet platform for its new vehicle. It needed a faster platform to process the massive amounts of data from both infotainment and ADAS features. The platform also had to ensure seamless connectivity between the legacy controller area network (CAN) bus, the local interconnect network (LIN) devices, and the new Ethernet platform.
The Challenges
Unlike the slower speed backplanes of CAN and LIN platforms, 100BASE-T1 automotive Ethernet requires rigorous compliance testing. This leaves no room for error, as any data packet received in error or delay could mean the difference between stopping at a traffic light or running a red light into oncoming traffic.
The car maker wanted to ensure 100% conformance to the IEEE 802.3bw-2015 standards for the 100BASE-T1 automotive Ethernet. Specifically, the car maker’s safety team wanted to validate the receiver (Rx) performance of a critical ethernet switch unit.
They faced two significant challenges:
The car maker had initially considered developing their BERT. They soon realized the process was very tedious and would delay their test development schedule by weeks. Aside from trying to understand the standards specifications correctly, they had to configure and run the required tests from the beginning. There was also the challenge of analyzing and measuring the results obtained from their device under test (DUT), and a manual comparison against the published specifications.
The car maker decided to turn to their existing test and measurement vendors for a solution.
The Solution
After competitive evaluations, the car maker chose Keysight’s E6962A Automotive Ethernet Rx Compliance solution, part of the Keysight suite of automotive Ethernet compliance solutions.
The Keysight solution included the following:
At a click of a button — test patterns were generated and transmitted to the DUT, and the automotive Ethernet Rx solution then received and automatically analyzed the test patterns to return the BERT pass or fail results.
The Results
Keysight’s solution enabled the car maker to ensure performance and compliance while keeping the project on schedule.
The car manufacturer’s safety team trimmed two weeks off their initial test development schedule with the E6962A software, which intuitively and quickly walked them through the test set-up and results.
×
Please have a salesperson contact me.
*Indicates required field
Thank you
A sales representative will contact you soon.
What are you looking for?