TDECQ Part 1: Making Accurate and Repeatable Compliance Measurements

White Papers

TDECQ is the acronym used to describe “transmitter dispersion and eye closure quaternary”. This is a power penalty metric that describes how much extra power is required from a transmitter, relative to an ideal transmitter, to compensate for both non-ideal transmitter waveforms and the impact of chromatic dispersion. It is similar to the transmitter dispersion penalty (TDP) metric used in NRZ optical communications standards. It was developed in the IEEE 802.3bs standard and improved in the IEEE 802.3cd standard. It is a convenient way to specify the performance of a PAM4 transmitter, as it aggregates many transmitter attributes into a single metric, and the metric directly indicates the impact a transmitter’s imperfections will have on overall system-level performance.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.