Signal Integrity Simulation Using ADS

Application Notes

Question

What is the benefit of S-parameter simulation? What components are specific for S-parameter simulation?

Answer

S-Parameters Simulator calculates wide band S-parameters of a channel. Term is used to define the impedance and location of the ports for S-parameters simulation. Term has to be continuously numbered from one. Note that time domain sources, IBIS, IBIS AMI and SPICE IO models are not compatible with S-parameters simulation.

S-Parameter Simulator supports not only S-Parameters, but also Z Parameters and Group Delay. You can check the items which you want to examine during simulation. Z parameter is used to analyze the impedance profile of the power distribution network (PDN). It is useful for power integrity analysis.

Channel bandwidth and Crosstalk can be extracted from S-parameter. Channel bandwidth limits maximum bit rate. Insertion loss to crosstalk ratio affects system BER. Both channel bandwidth and crosstalk are important design factors for SI. A simple S-parameter simulation of channels is shown in Figure 2. The results of Insertion loss and crosstalk are shown in Figure 3.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.