The Flash Programming Flow

Article Reprints

Keysight Technologies

The Flash Programming Flow

Article Reprint

The Flash programming Flow

On-board flash memory device testing and programming.

Memory capacities are one of the important prod-uct specifications consumers review before buying a product. An increasing number of memory devices are being packed into electronics products, and a single malfunction could cause gross failure across the devices. Hence, flash memory testing and program-ming have become indispensible to the quality check during different product development phases.

This month, we focus on how on-board flash memories are being tested and programmed at differ-ent stages of product development and manufactur-ing. (The term “on-board” refers to flash memory soldered into the PCB.)

Flash memories are programmed across differ-ent stages of the product, from engineering verifi-cation and production verification to high-volume manufacturing. During the prototype and engineering verification stages, the R&D and NPI test engineer tests and programs the on-board flash memories. The first step performed is structural test, to ensure that the flash memory is correctly soldered in the PCB and that there are no short or open defects on the flash memory pins.

One of the available boundary scan tools that has the capability to simultaneously test and program flash memory is the PC boundary scan device. This has the capability to generate structural test vectors able to verify that the addresses, control lines and data pins of the flash memory are correctly soldered on the PCB. Boundary scan tools make use of the IEEE 1149.1 standard for test access port and boundary scan archi-tecture, commonly known as JTAG.

The PC boundary scan tool offers some advan-tages worth considering:

  1. It is easy to implement during prototype by making use of the CPU/ASIC/FPGA boundary scan cell to test and program the flash memory devices connected.
  2. A bed-of-nails fixture is not needed. Instead, all that is needed are four mandatory pins on the boundary scan device: TDI, TCK, TMS, TDO and the optional TRST.
  3. New benchtop solutions enable tests or program-ming vectors developed during prototype and engineering verification to be used during product verification and volume manufacturing.

During product verification, depending on the test strategy used, the PCB with on-board flash mem-ory can be tested and programmed using in-circuit testers or a PC boundary scan tool. The latter can also be integrated directly into the ICT for boundary scan testing and flash memory device programming, and the same test developed for the prototype can be reused during engineering verification.

Ensuring on-board flash memory is programmed with the correct data.

There are two types of data that can be programmed into the flash memory:

  • Static data. The data are fixed and do not change.
  • Dynamic data. The data do change and vary from one PCB to another PCB.

It is not advisable to program large amounts of static data in the flash memory using boundary scan silicon nail or via direct programming using the ICT bed-of-nails, as the test time can be very long, and this might affect the production beat rate.

Static data can still be programmed into the flash, however, if they are only a few megabytes, as in those found in firmware needed to enable PCB boot up at the functional test stage, or when dynamic data programming is needed. These examples can be found in the creation of mac addresses, board serial numbers, time stamps, testing history and other variable data.

The on-board flash memory is cor-rectly soldered in the PCB

Any open or shorts failure in the flash memory pins might cause a gross failure at the functional test station, such as “no boot” or “hang” symptoms. This will be a failure that is hard to diagnose at the functional test station because other device failures can also exhibit the same symptoms. Besides, if the flash memory is not programmed properly, the PCB might not be able to boot up properly, and the functional test might not be able to proceed, thereby disrupting the rest of the functional test. However, at the ICT stage, the failing devices can easily be diagnosed and repaired, permitting the rest of the functional test to proceed.

The flash test executed at this stage is done using a simple walking one “1” or walking “0” test to toggle the address. The data bus is verified by writing a com-plementary set of data to ensure all pins are toggles. The control pins such as write enable and output enable of the flash memory are also checked to ensure the pins are correctly soldered on the PCB. This test can be executed either by using a PC boundary scan tool or an ICT during production testing.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.