Photodiode Test Using the Keysight B2980A Series

Application Notes

A photodiode (PD) is a semiconductor device that converts light into current. When the PD is reverse-biased, a current is generated as the PD absorbs photons. The PD also produces a small amount of current when no light is present; this is known as dark current. Since the output current is directly proportional to the light intensity applied to the PD junction, it can be used to detect small quantities of light. This makes PDs useful in a wide range of applications such as optical communication, light detection, and consumer electronics.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.