Impedance Matching in the Laboratory

Application Notes

The reception and transmission of small signals into amplifier stages and the transmission of large, powerful signals into loads both require careful attention to minimizing losses. At RF and microwave frequencies reflections of the propagating wave can drastically undermine the efficiency of transmitted power or the signal-to-noise ratio of transmitted information. Proper matching of impedances is needed to minimize these reflections and insure that any signal which reaches a load is actually absorbed by that load as useful power. Proper impedance matching is a fundamental skill that is central to all RF and microwave engineering. The ability to design and execute proper impedance matches is a crucial and highly sought skill which can make or break a career as well as a specific design. The mathematical elements of impedance matching have already been investigated using SPICE and other tools such as the Smith chart. In this lab, some practical laboratory approaches to the problem of impedance matching will be examined. Network analyzers are the essential tool for assessing and tuning an impedance match. Impedance matching is often viewed as a difficult art because impedance matching involves an interplay of measurements and design calculations. However, there are developed methods, and mastering these is essential to RF and microwave engineering. 

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.