High Attenuation Measurement of Step Attenuators

Application Notes

This paper introduces a solution for high attenuation measurement of step attenuators. Fundamentally, this high attention measurement method is based on the cascaded 2-port network and S-parameter theory; this method is to compute S-parameters of high attenuation (> 80 dB) using the measured S-parameters of lower attenuation (≤ 80 dB) settings, and the calculations depend on attenuator card sequence and physical structure of step attenuator. This method can measure the attenuation high as 120 dB.

 

This is NOT a straight dB addition, this solution can offer considerable accuracy only using VNA (Vector Network Analyzer), and it uses T-matrix (as known as transmission parameter or cascade parameter) method which can make the calculations easier. Measurement uncertainties are derived from uncertainties of cascaded S-parameters, for example, measurement uncertainty for 80 dB at 18 GHz is less than 0.8 dB and 110 dB at 18 GHz is less than 1.0 dB.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.