Basic RF Amplifier Test with the E5072A Network Analyzer

Application Notes

Characterizing RF Ampliiers – Measurement Parameters

S-parameters/stability factor

Traditionally, S-parameters (both relection and transmission) measurements have been performed with VNAs. As well as basic S-parameters of devices, designers and manufacturers have to carefully look into various parameters calculated from the S-parameters. K-factor is one of the examples and a signiicant parameter especially for ampliier designers. This factor can be calculated from all the S-parameters of two-port devices (S11 to S22), and represents the stability of ampliiers. When K-factor is greater than 1 while delta is smaller than 1, the ampliier is unconditionally stable and no oscillation is expected for any load.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.