Wireless LAN at 60 GHz – IEEE 802.11ad Explained

Application Notes

The first popular standards for wireless LAN (IEEE 802.11a and b) were designed primarily to serve the needs of a laptop PC in the home and office, and later to allow connectivity “on the road” in airports, hotels, Internet cafes, and shopping malls. Their main function was to provide a link to a wired broadband connection for Web browsing and email. Since the speed of the broadband connection was the limiting factor, a relatively low-speed wireless connection was sufficient – 802.11a provided up to 54 Mb/s at 5 GHz, and 802.11b up to 11 Mb/s at 2.4 GHz, both in unlicensed spectrum bands. To minimize interference from other equipment, both used forms of spread-spectrum transmission and were heavily encoded. A later revision of the standard, 802.11g in 2003, consolidated use in the 2.4 GHz band but maintained the maximum data rate at 54 Mb/s.