Using PrecisionProbe Software on the Infiniium 9000 Series Oscilloscopes to Correct for Probe Loss

Application Notes

Oscilloscope probes provide the vital link between an object to be measured and the oscilloscope. Because they are inherently lossy, probes influence both the accuracy of the measurement result and measurement repeatability. To compensate for the inherent loss, various techniques (e.g., probe correction via digital signal processing (DSP) or use of higher bandwidth probe heads) have been employed with mixed results. Over the last few years, waveform transformation software has made it possible to minimize the errors caused by the probing system, but the process is long and arduous. This application note introduces an easier and quicker solution for addressing the loss due to the probing system and its impact on oscilloscope measurements. The solution—the Keysight Technologies, Inc. PrecisionProbe software running on the Infiniium 9000 Series oscilloscopes—enables quick characterization of the entire probe system, making it increasingly more difficult for engineers to simply ignore the loss.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.