Application Notes
Connecting the Instruments
Two instruments can be synchronized only when cross-connected with a designated synchronization cable. To connect the cable, turn the power off on both instruments. Locate the rear-panel Master/Slave connector and attach each side of the cable to these connectors. Note that the connectors do not lock into position without screwing in the bolts on each side. Use a flat tip screwdriver to latch the cables into their receptacle housing, making sure the connectors are straight and firmly locked into place. Once the cable is connected, the instruments can be powered on again.
Resetting the Two Instruments
Once the two instruments have been connected using the synchronization cable, the next step is to perform a factory reset. Perform the following steps in both instruments:
×
Please have a salesperson contact me.
*Indicates required field
Thank you
A sales representative will contact you soon.
What are you looking for?