Application Notes
Since the release of the PCIe® base specification revision 3.0 (rev. 3.0) in November 2010, many semiconductor vendors have tested their bare ASICs accordingly. Now PCIe 3.0 add-in cards (AICs) and motherboards (MBs) with PCIe 3.0 slots are being developed. These items need to be tested according to the PCIe Card Electromechanical (CEM) Specification, for which the Serial Enabling Group (SEG) is currently generating the PHY Test Specification.
×
Please have a salesperson contact me.
*Indicates required field
Thank you
A sales representative will contact you soon.
What are you looking for?