Programming In-System versus Offline

Article Reprints

The decision rests on the line beat rate versus ICT test cycle time.

Modern electronics – cellphones, TV set-top boxes, laptops – contain at least one programmable device on board that usually contains boot-up or self-test firmware to enable these products to perform their functions properly. In general, there are two methods by which these devices are programmed: offline or in-system. 

How does one decide on offline programming or ISP? One key consideration is the cost of each method. Let us look at pros and cons of these two methods that contribute to the overall costing. 

First, let’s define each of these methods: 

  •  Offline programming. Device programming carried out independently of the actual production line before device is attached to the printed circuit board. 
  •  ISP. Device programming carried out in the actual production line; device is installed on the assembly before programming is performed. 

The sole benefit of programming offline versus in-system is that it takes out that time from the overall ICT test cycle time equation. If the SMT line beat rate is much faster than the overall ICT test cycle time, the ICT station will be a bottleneck for the production line.

Removing the programming portion from the ICT stage will improve the overall efficiency of the production line. The programming time depends on many factors, like the size of the data to be programmed, programmer clock speed, number of devices to be programmed, whether the program is implemented directly onto the device or via an upstream boundary scan JTAG port to program device, etc. 

On the other side of the coin, offline programming does have some big challenges. The first is inventory control. There will be multiple firmware versions across the customers’ range of products, and there will be even cases of multiple firmware versions for a single product with different functions turned on for different market needs.

Having offline programming for all these devices will require a good inventory control process. Imagine loading the wrong preprogrammed devices onto boards: the effort and cost of replacement would be tremendous.

The second challenge with offline programming is the inability to reprogram the device post-soldering. Often, firmware versions are frequently changed, especially during NPI. New firmware may be released during the production build, and the inability to reprogram the device online means one has to replace the device manually.

Or, if boards have been returned from repair, functional test or outside the factory, there usually are slight changes to the firmware, and the boards must be reprogrammed in the ICT. This reinforces that the ability to program in the ICT station is critical in a production environment. 

An offline programming station requires additional resources: operators, real estate, and of course the programming station itself. On the other hand, implementing ISP may require additional hardware or software on top of the existing ICT, not to mention development of the ISP solution. 

Simultaneous Programming

Performing programming on two similar boards simultaneously achieves two boards within one test cycle time. It can also mean programming two or more devices within the same board simultaneously, circuit topology permitting. How fast can ISP be? Consider real-time data I collected from two recent ISP projects. In both cases, the ICT was an Agilent Medalist i3070 Series 5 with plug-in cards.

EPIC’s DfM/DfT system prioritizes recommendations to make it easier for customers to understand how critical each recommended design change is to overall product quality. Documentation control is centralized to make sure production only has access to the most current revision of work instructions.

Design travelers accompany each work order to ensure that during shift changes or personnel changes there is a clear trail on what is being processed. Smaller batch sizes also contribute to minimizing this waste. 

Unnecessary inventory is also a challenging waste to minimize in the EMS environment. Unnecessary inventory comprises raw material, work-in-process and finished goods inventory.

While smaller lot sizes can minimize WIP, the relationships with customers found in EMS means forecasting and supply base choices are often a compromise between customer preferences and Lean best practices. Economy-driven variable demand further tests the system. 

In the EPIC model, the program manager starts by developing the customer order replenishment methodology. The tool for determining visibility into the customer’s demand is defined (i.e., ERP, EDI, etc.), and replenishment “pull” signals are defined.

Once these issues are addressed, initial finished goods kanban bin sizes are established. Trends are analyzed and bins resized as appropriate with customer approval. Strategic suppliers produce to the MRP forecast and ship to EDI release signals. Consignment, in-house stores and vendor managed inventory programs are used with strategic suppliers to maintain buffers closest to the point of use. 

Pipeline status or “bond” reports are regularly reviewed with supplier teams to ensure buffers and replenishment streams are able to support planned production within a range of variation based on past historical demand, current forecasts, customer service lead-time guarantees to their endmarket, manufacturing lead-times and transit lead-times. 

Like the wastes of transport and inappropriate processing, unnecessary or excessive motion costs money and slows throughput. And, as with the waste of inappropriate processing, customer reluctance to implement DfM/DfT recommendations can be a constraint in improving efficiency. 

EPIC’s automation strategies, DfM/DfT process and focus on designing factories with sequential processes all help improve efficiency, but ultimately, the most success in reducing this waste comes when customers are willing to adopt DfM/DfT recommendations.

Engaging the EMS provider during the design stage ensures optimal process efficiencies, translating to a successful and cost-effective product launch. 

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.