How to Add DC Offsets to a Function Generator's Output

Application Notes

A variety of electronic test applications require a DC offset to be added to the output of a function generator. The result is a signal that is a waveform superimposed on top of a DC voltage. For example, you can use a sine wave added on top of a DC bias voltage for testing a circuit’s immunity to noise that can appear on its real bias voltages. For amplifi er testing, you can bias a transistor with DC that has an AC component riding on top of it. Even a repetitive series of unipolar pulses, used for driving a FET gate signal for DC/DC converters, can be thought of as a pulse train with a DC offset. All of these applications need a DC plus AC signal, all with different voltage, current, and waveform bandwidth requirements.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.