Data Sheets
This Sensor Hub provides the interface for the Keysight Technologies, Inc. E1737A Material Temperature Sensor and Keysight E1738A Air Temperature/Pressure/Humidity Sensor used with the Keysight 5530 Laser Calibration System. Thesesensors monitor parameters in the environment of the device being calibrated to enable the laser system to calculate appropriate correction factors. The E1736A can accommodate multiple sensors of both types. The sensor hub interfaces with the system PC via a standard high-speed USB interface.
×
Please have a salesperson contact me.
*Indicates required field
Thank you
A sales representative will contact you soon.
What are you looking for?