Active Device Characterization with Keysight Mid-Range VNA

Application Notes

Introduction

 

Amplifiers and converters are essential components of RF and microwave sub-systems such as satellite transponders or radar transmit/receive modules. Noise figure is one of the key parameters that is characterized on the receiver component of these sub-systems.

 

Noise figure can be measured using test instrumentation such as a noise figure analyzer, spectrum analyzer, or a network analyzer. Network analyzers are often used due to other crucial measurement capability, such as S-parameters, gain compression, and intermodulation distortion. The network analyzer cold-source noise figure measurement technique available enables both accurate and efficient measurements.

 

During the design stage of a device, simplicity of testing (not requiring many external components) and speed of testing allow a designer to change and improve the design efficiently. In the manufacturing process, fast and simple testing allows for significant cost-savings.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.