Power Amplifier EVM Measurement with PNA-X Series Network Analyzer

Application Notes

PA in the wireless communication system

In wireless communication systems, PAs are located at the last stage of the transmission chain, to supply required RF power to antennas. The PA plays an important role, determining the quality of the communication service, in terms of signal quality and battery life. 

The PA is the biggest contributor to the quality of the RF chain in communication systems. Linearity is extremely important in systems with high peak-to-average-power (PAPR) signals, as in modern wireless standards where OFDM is used for the digital modulation scheme, because the nonlinear response of the RF chain directly impacts error in the demodulation, resulting in poor bit-error-rate. Also, spectral regrowth created by nonlinearity can create interference in other bands. Thus, maintaining linearity of the RF chain is critical for the quality of wireless communication.  

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.