Compliance Testing PCIe 5.0

White Papers

Data center operators need to embrace next-generation technologies to support the response times and high bandwidth requirements of 5G and IoT. With the expectation of billions of internet-connected devices and data-intensive real-time applications, 100 gigabit Ethernet (GE) speeds that are common in data centers today will not be fast enough. As a result, data center operators need to migrate their networks from 100GE to 400GE. Faster networking speeds require faster memory and faster serial bus communications.

In parallel with transceiver upgrades to 400GE, data center operators must transition to the next generation of high-speed computing interfaces. Double date rate (DDR) memory will move from DDR 4.0 to DDR 5.0, and Peripheral Component Interconnect Express (PCI Express® or PCIe®) expansion bus will move from PCIe 4.0 to PCIe 5.0.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.