Solar Maximum Power Point Tracking (MPPT) for IoT Devices

Application Notes

Internet of Things (IoT) devices are typically low-power, battery-operated devices, and the use of solar energy to power IoT applications and devices is also becoming more prevalent. The primary reason for using solar energy is because it is a clean and cost-effective renewable energy source. You don't have to change your battery as frequently after installing the solar panel.

 

A high-performance solar panel must not only provide consistent power to your IoT devices, but it must also be able to withstand harsh conditions and long-term UV exposure. Prior to selecting the right solar panel for your application, you must consider the solar panel's performance.

 

To evaluate the performance of a solar panel, you can start by profiling the current-voltage (I-V) and power-voltage (P-V) characteristic curves to determine if a solar panel is capable of providing the maximum amount of power required by your IoT device. This application note explains how to use an electronic load to determine the I-V curve, P-V curve, and MPPT of a solar panel for your low-powered IoT devices.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.