Measuring Leakage Current on the i7090 with 1.21p Software

Application Notes

What is Leakage Current?

Leakage current flows from either AC or DC circuit in equipment from both the input and output to the ground. It typically occurs when there is a fault in the insulation of electrical devices. There are several ways to measure a board's leakage current with an ICT, such as adding an SMU to the ICT. However, doing so can be costly. This application note discusses alternate solutions that use the latest feature from the 1.21p version software and a serial resistor to measure a DUT's leakage current.

 

Measuring Leakage Current

The standard practices for measuring leakage current using a serial resistor would typically require a battery on a board. In some cases, the battery may not even be present, or the user would like to measure it without the battery. Adding a serial resistor between a DUT's power supply and a power node on the board lets you measure the leakage current without the onboard battery.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.