E8719A Radar Target Simulator

Data Sheets

Today and Next Generation Radars

 

76 – 77 GHz band radars have been available in the market for many years now and is the dominant automotive radar sensor being manufactured today. In place of the older 24 GHz short range radars, the 77 – 81 GHz radars are gaining traction with a significant amount of investment placed to take advantage of the wider bandwidth (BW) giving the radar sensor the improved resolution and full imaging capability. Boosted further with advance processing capabilities and the inclusion of AI, the future is looking bright for automotive radar sensors. 

 

Target simulators

 

Be it long- or short-range radar sensors, the applicable frequency range from 76 – 81 GHz is wide. Test setups have been just-enough, most manufactured radar sensors at this point had a narrow BW, typically from 800 MHz to 1 GHz. As described above, this is quickly changing with increasingly wider BWs being applied. Keysight was among the first to release the 4 GHz wide target simulator from 77 – 81 GHz, and now expanding it further to cover the full 76 – 81 GHz with 5 GHz of instantaneous bandwidth and ready to take on the challenge of any radar sensor within this frequency band on the market.

 

E8719A radar target simulator

 

The Keysight E8719A Radar Target Simulator, with full 5 GHz of instantaneous bandwidth includes improved distance accuracy of 5 cm, aligning to the performance expectations from future imaging radars. A new over-the-air calibration feature has also been included to improve path loss and minimize uncertainties in radar test setups, please refer to the comprehensive E8719A Radar Target Solution Guide for more information.

 

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.