Spectrum and Network Management Convergence for Wireless Communications

White Papers

The main objective of this work is to study the spectrum-network management convergence that enables spectrum efficiency while providing adequate Quality of Service (QoS) required for mission critical applications running on a wireless communication network. We combine well known QoS frameworks with the different dynamic frequency (channel) allocation approaches for spectrum management to devise mechanisms that can enable efficient spectrum-network management in wireless networks with Joint Tactical Radio ystem (JTRS)-like nodes. Specifically, we present two schemes: the first is “GreedyDiffServ” scheme which is based on DiffServ and the opportunistic (greedy) approach for dynamic frequency allocation. The second scheme is “Shared Information-IntServ” which is based on IntServ and the shared information approach for dynamic frequency allocation. These two mechanisms are implemented in the QualNet network simulator on a hierarchical wireless mobile ad hoc network using “JTRS-like” devices and are evaluated against an extensive set of notional scenarios. We present simulation results that highlight the advantages of deploying a spectrum-network management scheme in a wireless network and compare the performance of the two mechanisms. 

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.