Fixture Reusability Consideration From In-line to Offline

Application Notes

The i3070 In-Circuit Tester (ICT) fixture is an electromechanical assembly comprised of a bed of nails that allows access to multiple test points on both sides of the printed circuit board (PCB). ICT will transmit test signals to and through the printed circuit board's access points to conduct structural tests on standard components and integrated circuits (IC).

This application note discusses the differences between the i3070 Series 5 in-line 4 module test system (E9986E) fixture and the offline 4 module test system fixture, as well as the considerations for fixture reusability.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.