Network Emulator 3: 100GE, 50GE, 40GE, 25GE, and 10GE Impairment

Data Sheets

Problem: Knowing How Networks and Devices Will Behave Under Real-world Conditions

 

Effective testing requires a real-world environment that reproduces realistic network conditions and behavior. All software and hardware should be subjected to a realistic test environment before deployment.

 

Solution: Real-World Network Impairment Testing

 

Network Emulator 3 (NE3) is a precision test instrument for 100GE, 50GE, 40GE, 25GE, and 10GE Ethernet impairment. The device allows users to accurately emulate the real network conditions that occur over live production LAN/WAN networks. By emulating realistic and worst-case network conditions in the lab, users can validate and test performance of new hardware, protocols, and applications to prevent failures in production networks. The Network Emulator 3 offers a rich featureset to allow testing in a controlled lab environment with repeatable and predictable impairments. The NE3 enables user to perform the following tests:

 

• Test 5G networks and the impact of delay and impairments

• Test the effect of delay on the network and application performance

• Determine how applications will perform when distributed across data centers

• Cause outage and degrade scenarios to trigger and validate fail-over protection

 

Highlights

 

Emulate real-world networks in the lab

• Enables validation, performance, and interoperability testing

• Test products and applications to characterize end user experience under real-world conditions

• Precisely reproduce and quickly resolve issues occurring in the field

 

Key features

 

• 100GE / 50GE / 40GE / 25GE / 10GE impairment emulation

• 1 or 2 impairment engines FPGA hardware architecture allows 100 % line-rate performance

• Test mixed speeds at the same time with one device

• Flexible resource management

• High port count 100GE, 50GE, 40GE, 25GE, and 10GE FPGA emulator

• FPGA hardware-based architecture provides maximum precision and accuracy • Modular appliance allowing impairment of one or two data lines

• One impairment engine per card enables impairment of one data line

• Optional second impairment card available 

• Dedicated FPGA processors per card ensures high performance

• Flexible Resource Management enables allocation of resources as needed by allowing automatic or manual memory allocation

• Precisely emulates delays and impairment that exist in Ethernet networks

• Transparent to any higher-layer L2/7 protocols

• Optical media physical layer clock transparency for SyncE support

• Test automation through RESTful Web API, which allows control by TCL and languages such as Python

• Packet Capture

 

Primary Use Cases

 

• 5G delay and impairment testing

• Performance testing of critical applications over Ethernet with realistic network conditions and impairments

• Combine with IxNetwork, IxLoad, and BreakingPoint test systems to create a complete real-world test environment 

• Real-world interoperability and customer proof-of-concept (PoC) testing 

• Corporate LAN/WAN emulation 

• Business continuity and disaster recovery testing

• Server consolidation/migration 

• Application cloud migration and storage extension

• Wireless/mobile delay and impairment simulation 

• Satellite network delay emulation

• Reuse and build proprietary or standard-based Layer 2–7 protocol filter with the Customizable Filter Library

• Cause outage and degrade scenarios triggering fail-over protection

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.