Wireless LAN Throughput Test Using IOT8700 Series

Application Notes

Basics of WLAN Client-Server Architecture

A typical network architecture consists of a client and a server. The connection between them can be wired or wireless, it does not matter as long as they are connected.

  • A client is the device that requests a service or resource from the server.
  • A server is a physical computer run services to serve the needs of other computers.

In simple words, client services request to the server where server services response to the client.

Access Point Mode and Station Mode

Typically, Wireless Local-Area Network (WLAN) devices can run in one of the two modes: Access Point mode or Station mode.

  • Station mode (STA) mode is normally what most people understand as normal mode for a WLAN device. A device will use station mode to join a network. It is just like your PC or mobile phone joining your home Wi-Fi network. In this case, your PC or your mobile phone will run in station mode. Other example of devices running in station mode are wearables, Internet Protocol television (IPTVs), and various IoT devices.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.