Bypass Link Conveyor Built-in i7090 and i3070 In-Circuit Inline Tester

Application Notes

An automated production line uses an external link conveyor to transport objects such as the Printed Circuit Board (PCB) from one station to another. In some instances, the production line may require two similar systems or more at a station to maximize the production output rate. In such a case, you must have an external bypass link conveyor to transport the PCB from the busy system to another available system to perform the task simultaneously. However, the external bypass link can be complex to design and difficult to implement. It could also significantly take up the floor space.

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.