5G FR2 Solution for MFG Test

Configuration Guides

Optimize Throughput

 

Controlling a DUT is essential to verify performance. Non-signaling test solutions are typically preferred in manufacturing environments because the DUT responds more quickly. However, these solutions cannot use signaling to control a DUT. Instead, the EXM-WB makes use of the control software of chipset vendors. The EXM-WB is endorsed in QDART and integration with other chipset vendors is in progress.

 

Decrease test time with sequencing and parallel test

 

Sequencing is one method of decreasing overall test time. A set of test steps is prepared in one sequence and then initiated with a single trigger. Test speed increases since fewer commands are used. The sequence analyzer of the EXM-WB solution supports 5G NR measurement sequences with varying power levels and frequencies.

 

Parallel test is another method of decreasing overall test time. The new V9065EM2E parallel analysis of multiple devices software application runs with or without the sequence analyzer to provide fast test speed. Test time is significantly reduced when data is analyzed while configuring the device for the next tests and acquiring the next sets of data.

 

Flexibly verify multiple devices

 

Connect once to test the RF performance of your 5G FR2 device. Many use cases are supported with the combination of the E6681A EXM-WB wireless test, the M1740A remote radio head (RRH), and optional OTA chamber with accessories. Choose the configuration that provides optimal throughput for your manufacturing area.

 

Configure Hardware

 

The E6681A EXM-WB wireless test set hardware includes the following capabilities by default.

 

• Frequency ranges of 24.25 to 29.5 GHz and 37 to 43.5 GHz

• Chassis, reference, and embedded controller

 

Select transceiver and bandwidth options

 

Start by configuring the first transceiver, then add and configure one more transceiver, if desired. Each transceiver has three bandwidth options.

 

Option number

Description

Requirements

E6681A-001

Transceiver 1

Mandatory

• E6681A-B3X

Bandwidth, 300 MHz

Default

• E6681A-B6X

Bandwidth, 600 MHz

Optional

• E6681A-B12

Bandwidth, 1.2 GHz

Optional

E6681A-002

Transceiver 2

Optional

• E6681A-B3X

Bandwidth, 300 MHz

Default

• E6681A-B6X

Bandwidth, 600 MHz

Optional

• E6681A-B12

Bandwidth, 1.2 GHz

Optional

 

Select remote radio head options

 

At least one remote radio head is required. More than one can be purchased depending on the desired configuration.

 

Option number

Description

Requirements

M1740A

mmWave transceiver for 5G

Mandatory

M1740A-CA4

RF cable N-SMA 4m

Two are mandatory for each

M1740A ordered

M1740A-CB4

RF cable TNC-SMA 4m

One is mandatory for each

M1740A ordered

 

Configure Software

 

The E6681A includes the following by default.

 

• V9060EM0E IQ analysis measurement software

• V9065EM1E sequence analyzer for device applications

• Perpetual, node-locked licenses with 12-month support for every application selected

×

Please have a salesperson contact me.

*Indicates required field

Select a preferred method of communication*Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By continuing, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you

A sales representative will contact you soon.